Cable Marking Kit
2700 high-quality slide on PVC cable markers that includes letters, numbers and symbols.

For utilities, time is everything in this demanding and dangerous environment, so having the right product or solution available to keep your site running is essential. From sensors and valves for water treatment, to measurement and cables for power quality and distribution, RS can provide the complete solution, including tools and safety equipment.
We are constantly expanding our offer with the latest solutions from the leading industrial brands.
2700 high-quality slide on PVC cable markers that includes letters, numbers and symbols.
RCD protected combination switched socket outlets, that are IP67 rated
Polyester enclosures designed for harsh conditions and outdoor environments.
Wago 221 Compact splicing connectors for all wire types. 40% smaller, tool free lever operated.
IP67 Enclosed Switch disconnectors, available as 2 or 3 pole.
Control events in industrial automation systems, using Near Field Communication.

Power distribution is a key critical component from transmission systems through to workplace and individual homes, since if the equipment fails or stops then so does the revenue. Effective maintenance (planned or predictive) helps protect operational performance by delivering a safe and reliable supply. At RS we support the power distribution industries, by offering thousands of products from different technologies and leading brands to support and maintain the assets within power distribution, from cables and connectors, through to circuit breakers and power meters.

In the past, facility managers judged the state of electrical power quality in their facilities based on whether the lights were on or not. If the lights were on, power quality was good. If the lights were off and the occupants were complaining, then power quality was bad. A major concern facility managers have related to electrical power is how much it costs to keep the facility running. To that end, any opportunity to reduce energy consumption is an opportunity to improve efficiency. The typical approach to reducing energy consumption is to upgrade equipment to more energy-efficient models and to reduce energy usage patterns by staff and operations. What’s harder to identify, and what frequently gets lost in all the chatter, is the potential efficiency gain of improving power reliability and preventing the lights from ever going off. Thankfully, the potential causes of power reliability issues are well known and relatively easy to identify. A facility manager and electrical team can determine the level of risk they likely face compared to the level of risk they are comfortable with, and using measurement data they can make the best maintenance decision for the organization’s bottom line.

For efficient maintenance within water or waste water treatment areas, RS has the product range to help provide the solutions to maintain your infrastructure and keep your essential services flowing smoothly. Our wide offer from leading brands includes products from industrial pipeline and pumps, to sensors, valves and tools.

The Internet of Things (IoT) is transforming the way we work, allowing businesses to connect and monitor equipment from almost anywhere. Innovation within the utilities industry is happening through Smart Grid technology, which allows two-way digital communication between power provider and users, so that everything on the grid from power plant to individual appliances can be seen and controlled in real time, which means:
Manage costs & improving efficiency – power can be monitored and controlled on-demand. As energy requirements change during peak and off-peak demands, so do energy prices which reflect the costs to produce it in real time (only produce energy when it is needed – efficient and environmentally sound).
Preventative maintenance – sensors can be used to monitor changes in operating conditions, such as the increase current, temperature, vibration, etc. which intern can identify issues before equipment fails and allows preventative maintenance can be carried out at the optimum time.

RS Pro gives you an ever-expanding choice of around 40,000 quality-tested products engineered for demanding manufacturing and industrial environments. Below are just some highlights from our range that we have selected for our Utilities Customers.
Choose quality, performance and value without compromise.